SLYA094 August 2025 LM5137F-Q1
The switch node and output ripple voltage waveforms are shown in Figure 3-6 to Figure 3-10.
Figure 3-8 PFM + Phase Shedding, Switch Node at 0.5A Load
Figure 3-10 PFM + Phase Shedding, Switch Node at 1.2A Load
Figure 3-7 PFM + Phase Shedding, Switch Node at 0A Load
Figure 3-9 PFM + Phase Shedding, Switch Node at 0.8A LoadPMP41158 achieves excellent light load efficiency by shedding the phases at light load and minimizing current draw from the input supply. This results in only one phase operating under no load conditions, as Figure 3-7 shows. And as load increasing, the phase can start to work one by one, as Figure 3-8 to Figure 3-10 shows. In addition to phase shedding, the LM5137-Q1 operates in PFM mode. Refer to Figure 3-11 for light load efficiency performance.