SNAA439 April 2025 LM74502
Power tools are used in various industrial and household applications such as drilling, grinding, cutting, polishing, driving fasteners, and so forth. Cordless power tools use battery power to drive DC motors, and products are available in different power levels.
For a high current level application, this is typical to place a switch between battery and motor driver to make sure of safe operation when connecting or disconnecting power supply. Also, turning off the switch can reduce quiescent current of equipment, thus saving power during shipping status.
Traditionally, mechanical switches are used in this scenario due to simplicity and low cost. However, the switches are not reliable enough. Frequent switching affects the life of mechanical switches. Electric arc can be triggered during switching, which can do harm to other devices on board.
To avoid the problem caused by mechanical switches, electrical MOSFET switches can be used. Since motor inverter usually consists 6 MOSFETs to drive three-phase brushless DC (BLDC) motors, this additional MOSFET switch is usually called the seventh MOSFET (7MOS).
Figure 1 7MOS in Cordless Power Tools System7MOS can be implemented in different ways. To select the appropriate design, go through this section to identify your need.
MOSFET can be divided into two categories: N-channel MOSFET (NMOS) and P-channel MOSFET (PMOS). Both can be used as a switch. Compared with PMOS, NMOS is popular for lower cost and lower power consumption due to lower RDS,ON, and smaller size to realize the same current rating. Therefore, this application brief only talks about designs with NMOS.
Note that NMOS needs to be driven by a positive VGS, which means the gate voltage needs to be higher than the source voltage to turn on the switch. If NMOS is placed at high side, the source voltage equals to the supply voltage, and therefore the gate voltage needs to be higher than supply. To achieve this gate voltage, additional driver circuit is required.
| RDS,ON | Cost | Driver Circuit Design | |
|---|---|---|---|
| NMOS | Low | Low | Extra design needed in high-side control |
| PMOS | High | High | Simple |
Usually, battery management and motor control are implemented on two different boards, where battery management board is placed near battery (battery-side), and motor control board is positioned around motor (motor-side). The 7MOS switch can be installed on either board.
Wherever the switch is placed, the switch can add to PCB size, power consumption and heat. To decide the switch position, you need to consider which side can tolerate the deterioration of these specifications.
Figure 2 7MOS Placement: Battery-side
Figure 3 7MOS Placement: Motor-sideControl Method: High-Side or Low-Side?
At battery side, 7MOS can be placed between the supply and the load (high-side) or between the load and the ground (low-side).
Figure 4 Battery-side 7MOS Control
Figure 5 Battery-side 7MOS Control When implemented at low-side with NMOS, the switch does not require a gate voltage higher than supply to turn on, which saves the cost and area for additional circuit. However, the drawback is that when the switch is off, the ground reference for other parts of circuits (communication, motor driver, and so on) is lost. The floating ground is not safe, and isolation is required for communication in this case.
Although high-side NMOS switch needs driver circuit to generate voltage higher than supply, this implementation can maintain the same ground reference across the system all the time.
| Ground Reference | Driver Circuit Design | System Cost | |
|---|---|---|---|
| High-side NMOS control | Maintained all the time | Need to generate voltage higher than supply | High |
| Low-side NMOS control | Cut off when NMOS is off | Simple | Low |
Driver circuit is required to generate the control signal for 7MOS. Some battery management IC has already integrated the FET driver, while others need external circuit to realize this function.
Whether the driver circuit is integrated in battery management IC or not, this has to be low-power. At battery-side, the board power consumption is under tight control in shutdown mode to achieve low loss of battery power during shipment or long-term storage.
Battery management ICs with integrated FET driver have already taken the power of driver into consideration during the design stage. Therefore, achieving the low-power goal. Plus, the integrated driver saves the cost, board size, and extra effort to design circuit.
External driver circuit for low-side control can be built with low-cost passive devices to transfer control signal from MCU. The circuit is low-power, but consumes some PCB area.
In the design of extra driver circuit for high-side control, a driver device is usually used to generate control voltage higher than supply, which simplifies design and reduces area. This driver device requires careful selection to keep the power consumption under control in shutdown mode. Passive devices are still needed to build peripheral circuit for IC. The driver device can be configured with extra protection features (over-voltage protection, over-current protection, etc.), but adds to the total cost.
| Control Method | PCB Size | Main Cost | |
|---|---|---|---|
| Integrated FET driver | High-side | Small | Battery management IC |
| Low-side | Small | Battery management IC | |
| External FET driver | High-side | driver device (small) + passive devices (medium) | Battery management IC + driver device |
| Low-side | passive devices (medium) | Battery management IC |
Figure 6 FET Driver for Battery-Side
Figure 7 FET Driver for Battery-Side At motor side, the situation is similar with that at battery side. You can use either high-side or low-side control for 7MOS, with less limitation on power consumption in shutdown mode.
For low-side control, since motor driver IC usually does not integrate low-side MOSFET driver, external driver circuit can be built with low-cost passive devices as in battery-side 7MOS.
For high-side control, motor driver ICs usually integrate FET drivers to drive the high-side NMOS in motor inverter. The driver structure varies in different motor driver ICs. Some support extra load current while some don’t. For those supporting extra load, high-side control only needs simple peripheral circuit with low-cost passive devices. For those not supporting extra load, extra driver must be used. This driver can be implemented by driver device or passive circuit. Driver device is more compact in size than passive circuit, and can have extra protection features, but costs more.
Figure 8 FET Driver for Motor-Side 7MOS: High-side
Figure 10 FET Driver for Motor-Side 7MOS: low-side
Figure 9 FET Driver for Motor-Side 7MOS: High-side| Driver Structure | PCB Size | Main Cost | |
|---|---|---|---|
| High-side | Support extra load | Passive devices (medium) | Motor driver IC |
| Not support extra load | Driver device (small) + passive devices (medium) | Motor driver IC + driver device | |
| Driver circuit (large) + passive devices (medium) | Motor driver IC | ||
| Low-side | None | Passive devices (medium) | Motor driver IC |
High-side power switch ICs have charge pump inside to generate voltage higher than supply. When configured as 7MOS controllers, the switch can be triggered by signal from MCU and output gate voltage at the corresponding pin. The switches are easy to implement and have high integration to save PCB area. This design is useful when not wanting to change other ICs on the board.
Although many power switches integrate the MOSFET, heat dissipation can be a problem since the peak current in power tools application can reach tens of amperes. Therefore, power switches with discrete NMOS are designed for this application.
Figure 11 7MOS Control With Power Switch (LM74502)Different types of IC integrate various protection features as well, such as reverse polarity protection (RPP), reverse current blocking (RCB), overvoltage protection (OVP), undervoltage lockout (UVLO), overcurrent protection (OCP), and so on.
Two types of power switch are recommended: ideal diode/ORing controllers and hot swap controllers. When selecting the device, take the following specifications into consideration: input voltage, power consumption, package area, cost, and protection features you need.
| Part Number | Input Voltage (V) | Shutdown Supply Current (uA) | Package Area (mm2) | Cost | Protection Features |
|---|---|---|---|---|---|
| LM74502 | 65 | 1.5 | 8.12 | Low | RPP, UVLO, OVP, and so on |
| LM74500-Q1, | 65 | 1.5 | 8.12 | Low | RPP, UVLO, and so on |
| LM5050-1 | 80 | 475 | 8.12 | Medium | RPP, RCB, and so on |
| LM5060 | 65 | 15 | 14.7 | Medium | OVP, UVLO, OCP, and so on |
As discussed previously, a main challenge to realize high-side 7MOS control is to generate a gate control voltage higher than supply. This section focuses on solving this challenge.
The following methods can be considered:
Motor-side
Battery-side
Most BLDC motor driver ICs integrate a charge pump or bootstrap structure to turn on the high-side NMOS in the motor inverter. This part of circuit can be reused to control 7MOS as well.
This design is already described in the application note Cut-Off Switch in High-Current Motor-Drive Applications. The VCP pin of motor driver ICs can offer Supply + 10V to turn on the 7MOS with the help of low-cost but area-consuming discrete circuit.
Figure 12 7MOS Control With Motor Driver IC (Integrated Charge Pump)The bootstrap architecture alone cannot be used to generate Supply + 10V to control 7MOS, because this relies on the switching operation of motor inverter to maintain a constant voltage. A trickle charge pump is used in TI devices with bootstrap architecture to provide high-side NMOS gate voltage (Supply + 10V) when the input PWM duty cycle is close to 100%(Like DRV8328 and DRV8329). However, the trickle charge pump can withstand very light current load, which makes this difficult to drive the 7MOS directly. We can use a driver circuit to drive the 7Mos ,below is a exmple to use DRV8328 and driver circuit to drive the 7Mos :
Figure 13 7MOS Control With Motor Driver IC (Integrated Bootstrap)Resistor R1, R2, R3 and R4 needs to be chosen carefully since the resistors can form an unwanted path from bootstrap architecture to VBUS and carry load current.
Also, a large resistor value is preferred to relieve the load current burden of trickle charge pump. Also, high resistance makes the circuit vulnerable to noise and interference, and slows down the switching time.
For demonstration, R1, R2, R3 and R4 are chosen at MΩ level. In real application, smaller resistor value (100kΩ level) can be chosen, but the low-side NMOS in the inverter needs to be turned on first for a while to make sure the bootstrap capacitor is fully charged.
A demonstration circuit is built and the test result is shown in Figure 14, where Channel 1 is the MCU control signal, and Channel 2 represents the drain voltage of high-side NMOS in motor inverter (VBUS):
Figure 14 Turn On 7MOS With Driver Circuit
Figure 15 Turn off 7MOS With Driver CircuitWhen 7MOS is turned on, the battery supply (15V) is connected to motor inverter, and VBUS equals to supply voltage; when 7MOS is turned off, the battery supply is disconnected, and VBUS is pulled down to a low voltage level by a load resistor to ground. Therefore, the MCU can successfully control the 7MOS to connect or disconnect the supply with this driver circuit.
The demonstration design is built with low-cost passive devices and JEFTs, but this consumes about 30mm×30mm PCB area, which can be a concern for compact size design.
The above is just an example. In this case, the MOS cannot be turned on and off very quickly and cannot support fully 100% duty operation. We need to pay attention to this.
Table 6 lists the recommended devices:
| Part Number | Driver Structure | Maximum Input Voltage |
|---|---|---|
| DRV8320, DRV8323 | Charge pump | 60V |
| DRV8350, DRV8353 | Charge pump | 100V |
| DRV8328, DRV8329 | Bootstrap | 60V |
| DRV8334 | Bootstrap | 60V |
| DRV8161, DRV8162 | Bootstrap | 100V |
For motor driver IC with bootstrap architecture, future products of TI can upgrade the driver design to support higher load current and enable smaller size of peripheral circuit.
As discussed in FET Driver: Integrated or External? low-power devices must be used at battery side to save battery power in shutdown mode. To achieve this, designer can use either battery protector with driver function or low-power power switch.
TI’s battery protector BQ76200 consumes less than 9.5uA in shutdown mode. This integrates a charge pump and can be controlled by signal from outside (MCU or battery monitor), which matches the requirement of 7MOS control.
Low-power power switches introduced in 7MOS Control with Power Switch can also be used here. With shutdown current consumption less than 20uA, these devices can also hold the power budget under control.
| Part Number | Type | Shutdown Supply Current (uA) | Maximum Input Voltage (V) | Package Area (mm2) | Cost | Protection Features |
|---|---|---|---|---|---|---|
| BQ76200 | Battery protector | 9.5 | 27.5 | 32 | High | None |
| LM74500-Q1, LM74501-Q1, | Ideal diode | 1.5 | 65 | 8.12 | Low | RPP, UVLO, and so on |
| LM74502 | Ideal diode | 1.5 | 65 | 8.12 | Low | RPP, UVLO, OVP, and so on |
| LM74700-Q1,LM74701-Q1 | Ideal diode | 1.5 | 65 | 8.12 | Medium | RPP, RCB, UVLO, and so on |
| LM5060 | Hot swap controller | 15 | 65 | 14.7 | Medium | OVP, UVLO, OCP, and so on |
7MOS provides a reliable way to connect or disconnect power supply of cordless power tools. 7MOS can be implemented by an NMOS transistor with either high-side or low-side control. The main challenge to realize high-side control is to generate a gate voltage higher than supply. Table 8 summarizes TI’s designs to 7MOS control and compares performance.
| TI Design | Architecture | Recommended Devices |
|---|---|---|
| Motor-side | ||
| Control with power switch (ideal diode/ ORing controllers) | motor driver and power switch | LM74502, LM7450x-Q1, LM7470x-Q1,LM5050-1 |
| Control with power switch (hot swap controller) | LM506x, TPS249x | |
| Control with motor driver IC (charge pump) | motor driver | DRV8320, DRV8323, DRV8350, DRV8353 |
| Control with motor driver IC (bootstrap) | DRV8328, DRV8329, DRV8334, DRV8161, DRV8162 | |
| Battery-side | ||
| Control with battery protector | battery monitor + battery protector | BQ76200 |
| Control with low-power power switch | battery monitor + power switch | LM74502, LM7450x-Q1, LM7470x-Q1,LM5060 |
| Control with battery monitor | battery monitor | High-side: BQ769x2 |