SNLU197A February   2016  – August 2026 DP83867CR , DP83867CS , DP83867E , DP83867IR , DP83867IS

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1USB-2-MDIO Description
    1. 1.1 Components Needed for USB-2-MDIO Setup
  5. 2Flashing MSP430 Launchpad
  6. 3Hardware Setup
    1. 3.1 Power Sequencing
  7. 4USB-2-MDIO Setup
    1. 4.1 Creating a Script
    2. 4.2 Opening and Running a Script File
    3. 4.3 Saving Data Results
  8. 5Off-Board Flash Setup
  9. 6Revision History

USB-2-MDIO Setup

The USB-2-MDIO GUI allows communication to 32 different PHY IDs, register access to extended registers and standard registers, running scripts, and saving register data. After the above flashing and hardware connections have been completed, follow the procedure below to enable register access through USB-2-MDIO:

  1. Open USB-2-MDIO and navigate to 'Settings.'
    1. Set the COM port as the 'USB Serial Device' COM port that appears in device manager.
    2. Set the Baud rate to 9600.
    DP83867CR DP83867CS DP83867E DP83867ERGZ-S-EVM DP83867IR DP83867IS ETHERNET-SW USB-2-MDIO USB2MDIO
                            Settings Figure 4-1 USB2MDIO Settings
  2. Press the 'Open Port' button. The port status panel shows 'HW Connected.'
  3. Open the PHY ID dropdown and select the PHY MDIO/MDC address to target.
  4. Enter the register address to read within the Register Address text field. This must be a 4-digit hex value, such as 0000.
  5. Press the 'Read' button. The bottom text panel shows the value contained within the register.
    DP83867CR DP83867CS DP83867E DP83867ERGZ-S-EVM DP83867IR DP83867IS ETHERNET-SW USB-2-MDIO USB2MDIO Read Figure 4-2 USB2MDIO Read
  6. To write to a register, enter the register address within the Register address text field and enter the value to be written in the 'Data' text field.
  7. Press the 'Write' button. The bottom text panel shows the new value contained within the register.
    DP83867CR DP83867CS DP83867E DP83867ERGZ-S-EVM DP83867IR DP83867IS ETHERNET-SW USB-2-MDIO USB2MDIO Write Figure 4-3 USB2MDIO Write

If the bottom text panel shows an error when reading or writing registers, verify the COM port and PHY address are set correctly. If these checks do not show issues, restart the USB-2-MDIO software and power cycle the MSP430 launchpad. Restarting the PC can help as well.