For the GUI to properly work with the MSP430F5,
the correct firmware needs to be installed on the microcontroller by following the
procedure below.
- Make sure the MSP430 launchpad is configured as
shown in Figure 2-1.
- Connect the MSP430
launchpad to a PC using a USB micro-B cable. Note that MSP430 drivers are required to properly connect the
MSP430 LaunchPad.
- Open Uniflash:
- If the launchpad is
detected under 'Detected devices,' press 'Start'
- If not, manually
configure by:
- Searching 'F5529'
and select MSP-EXP430F5529LP.
- Select TI MSP430
USB1 and press 'Start.'
- Load the USB-2-MDIO firmware text file by pressing 'Browse,'
navigating to this file, and selecting 'Load Image.'
- If prompted to update or
flash EZ-FET, do so. MSP flashing follows shortly after.
- After successfully loading the image, device
manager must show three COM ports when the MSP430 launchpad is connected. The
correct COM port for USB-2-MDIO to target is shown as 'USB Serial Device.'The launchpad is now flashed correctly for USB-2-MDIO. Power cycling the
launchpad can help to show the correct target COM port if not seen after
flashing.