SNLU353 October 2024
The ASPEED Ethernet EVM also contains a manual reset button which causes a hard-reset of all PHYs when pressed. This is achieved by driving the active-low pins of each PHY to LOW. The reset circuitry also has an automatic reset that is triggered when VCC (OVDD_3V3) falls below 2.93V.
Figure 3-6 Manual Reset Push Button