SNLU353 October 2024 DP83867CR , DP83867CS , DP83867E , DP83867IR , DP83867IS , DP83869HM
Finally, from the Tera Term console, run the following command:
Figure 2-1 mactest Output for 1 Gbps MAC
Interface.
As seen in the figure below, there are small pockets of useable delay settings depicted by the rectangular areas containing the "." character. These pockets show the user where the delay settings meet the timing requirements of the PHY. Additionally, for 100 Mbps tests, these pockets are larger in area because the timing requirements are more relaxed.