SNOS773P March 2000 – February 2025 LP2981-N
PRODUCTION DATA
The new chip has an output pulldown circuit. The output pulldown activates in the following conditions:
Do not rely on the output pulldown circuit for discharging a large amount of output capacitance after the input supply has collapsed because reverse current can flow from the output to the input. This reverse current flow can cause damage to the device. See the Reverse Current section for more details.