SNOU203A May 2024 – December 2024 TMP118
The EVM is divided into three sections: the controller section, the breakable FPC Connector section and the FPC Board containing the TMP118 sensor. The breakable sensor portion can be detached to use the sensor in the following scenarios:
The figure below highlights the EVM sections as well as some components that must be identified by the user to understand the purpose and use. The components are further explained in detail in the sections below.