SNVA940 November 2021 LM5157 , LM5157-Q1 , LM51571-Q1 , LM5158 , LM5158-Q1 , LM51581 , LM51581-Q1
With the given design parameters, selecting the proper switching frequency is the first step in the design process. In general, a higher switching frequency yields a smaller solution size at the cost of a higher switching loss and lower efficiency. Therefore, the final selection of the switching frequency is a trade-off between the power density and efficiency based on the specific requirement of the application. Harmonics of the switching frequency should be considered in designs that have strict EMC requirements. Equation 1 is used to set the frequency of the oscillator in the LM5157x and LM5158x. The example application is selected to have a switching frequency of 2.1MHz.
A standard value of 9.53kΩ with 1% tolerance is chosen for RT.
The internal oscillator of the LM5157x and LM5158x can be synchronized to an external clock as described in the data sheet. The LM5157x and LM5158x has a maximum duty cycle limit that is frequency dependent, which is also characterized in the data sheet.