The PCB layout of any DC/DC converter is critical to the optimal performance of the design. Bad PCB layout can disrupt the operation of an otherwise good schematic design. Even if the converter regulates correctly, bad PCB layout can mean the difference between a robust design and one that cannot be mass produced. Furthermore, the EMI performance of the regulator is dependent on the PCB layout to a great extent. In a buck converter, the most critical PCB feature is the loop formed by the input capacitors and power ground, as shown in Figure 8-48. This loop carries large transient currents that can cause large transient voltages when reacting with the trace inductance. These unwanted transient voltages disrupt the proper operation of the converter. Because of this, the traces in this loop must be wide and short, and the loop area as small as possible to reduce the parasitic inductance. Figure 8-49 and Figure 8-50 show recommended layouts for the critical components of the LM636x5D-Q1.
- Place the input capacitors as close as
possible to the VIN and PGND terminals. VIN and PGND pins are adjacent,
simplifying the input capacitor placement. Thermal reliefs in this area are not
recommended.
- Place a bypass capacitor for VCC close to the
VCC pin. This capacitor must be placed close to the device and routed
with short, wide traces to the VCC and PGND pins. Thermal reliefs in this area
are not recommended.
- Use wide traces for the CBOOT
capacitor. Place CBOOT close to the device with short and
wide traces to the BOOT and SW pins. Thermal reliefs in this area are not
recommended.
- Place the feedback divider as close as
possible to the FB pin of the device. If an external feedback divider is
used with the ADJ option, place RFBB, RFBT, and
CFF close to the device. The connections to FB and AGND must be
short and close to those pins on the device. The connection to VOUT
can be somewhat longer. However, this latter trace must not be routed near any
noise source (such as the SW node) that can capacitively couple into the
feedback path of the regulator.
- Use at least one ground plane in one of the
middle layers. This plane acts as a noise shield and also act as a heat
dissipation path.
- Connect the thermal pad to the ground
plane. The thermal pad (DAP) connection must be soldered down to the PCB
ground plane. This pad acts as a heat-sink connection and an electrical ground
connection for the regulator. The integrity of this solder connection has a
direct bearing on the total effective RθJA of the application.
Thermal reliefs in this area are not recommended.
- Provide wide paths for VIN, VOUT, SW, and
PGND. Making these paths as wide and direct as possible reduces any
voltage drops on the input or output paths of the converter and maximizes
efficiency. Thermal reliefs in this area are not recommended.
- Provide enough PCB area for proper
heat-sinking. As stated in Maximum Ambient Temperature, enough copper area must be used
to make sure of a low RθJA, commensurate with the maximum load
current and ambient temperature. The top and bottom PCB layers must be made with
two-ounce copper and no less than one ounce. Use an array of heat-sinking vias
to connect the thermal pad (DAP) to the ground plane on the bottom PCB layer. If
the PCB design uses multiple copper layers (recommended), these thermal vias can
also be connected to the inner layer heat-spreading ground planes.
- Keep the switch area small. Keep the
copper area connecting the SW pin to the inductor as short and wide as possible.
At the same time, the total area of this node must be minimized to help reduce
radiated EMI.
See the following PCB layout resources for additional important guidelines: