SNVSC27B October 2022 – January 2025 TPS38700
PRODUCTION DATA
The TPS38700 is designed to
give an accurate CLK32K output and it is used internally for setting the RTC time and
alarms. TPS38700 is configured to be used with a 32.768kHz crystal
oscillator. To achieve a well-defined frequency of oscillations, all crystals oscillators
are tuned at specific capacitive load such as 6.5pF, 12pF, or
20pF (during manufacturing stage), which becomes a part of
the crystal specification. The task of a designer is to design within the crystal's
specifications to achieve the correct specified frequency.
For these crystal oscillators, the need for loading capacitors are required because the capacitive load is effectively split between the output and input capacitance in a typical Pierce Oscillator scheme. These capacitors are essentially connected in series with the crystal oscillator. Therefore, if a chosen crystal oscillator has a capacitive load that is specified for 12.5pF load, then the need for two 12.5pF capacitors are required for proper frequency output from the crystal oscillator.
The TPS38700 is configured to be used without the need of loading capacitors, as long as the 6.5pF version of the external crystal oscillator is selected. External crystal oscillators will typically specify their internal capacitance such as 6.5pF, 9pF, 12.5pF etc. If the external crystal oscillator has load capacitance specification requirement not equal to 6.5pF, please contact the TI factory for an OTP (one time programming) configuration for the correct external capacitor loading.
The CLK32K signal can start as late as 50ms from when the input voltage VDD exits out of UVLO. The accuracy of CLK32K is within ±100ppm after one second of initial operation. If the frequency of CLK32K deviates for more than ±10%, a fault interrupt is asserted. The accuracy of the CLK32K will also depend on the choice of external crystal oscillator and its temperature rating.