SNVSCN3A April 2025 – May 2026 TPS371K-Q1
ADVANCE INFORMATION
The TPS371K-Q1 has a Built-In Self-Test (BIST) feature that runs diagnostics internally in the device. This feature is only included in certain variants, check the Section 9.1 to verify variant features.
BIST Diagnostics:
Startup BIST is initiated automatically after crossing VDD(min). During power-up, the BIST test asserts and holds OUT OV, OUT UV, LOW UV, and BIST low until the BIST test completes successfully. The length of the BIST is specified by tBIST. If BIST is not successful due to the internal blocks not working properly, the BIST is held low signifying a fault internal to the device. See Figure 7-6 for more details.
After a successful power-up sequence, BIST can be initiated any time with a positive edge transition on the BIST EN pin. BIST only initiates if the SENSE pin is not in a fault mode. During this BIST test time period, tBIST, BIST pin asserts low to signify that BIST has started and OUT OV, OUT UV, LOW UV assert. During BIST the device is not monitoring the SENSE pin for faults and the OUT OV, OUT UV, LOW UV pin is not dependent on the SENSE pin voltage. Upon successful BIST the BIST pin and OUT OV, OUT UV, LOW UV pin are deasserted. If BIST is not successful due to the internal device not working properly, the OUT OV, OUT UV, LOW UV pin and BIST pin are asserted low signifying a fault internal to the device. See Figure 7-7 and Figure 7-8 for more details.