The PCB layout of any DC/DC converter is critical
to the optimal performance of the design. Bad PCB layout can disrupt the operation
of an otherwise good schematic design. Even if the converter regulates correctly,
bad PCB layout can mean the difference between a robust design and one that cannot
be mass produced. Furthermore, the EMI performance of the regulator is dependent on
the PCB layout to a great extent. In a buck converter, the most critical PCB feature
is the loop formed by the input capacitors and power ground, as shown in Figure 8-26. This loop carries large transient currents that can cause large transient
voltages when reacting with the trace inductance. These unwanted transient voltages
disrupt the proper operation of the converter. Because of this disruption, the
traces in this loop must be wide and short, and the loop area as small as possible
to reduce the parasitic inductance. Figure 8-27 shows a recommended layouts for the critical components of the LM63635C-Q1.
- Place the input capacitors as close as
possible to the VIN and PGND terminals. VIN and PGND pins are adjacent,
simplifying the input capacitor placement. TI does not recommend thermal reliefs
in this area.
- Place a bypass capacitor for VCC close to the
VCC pin. Place this capacitor close to the device and routed with short,
wide traces to the VCC and PGND pins. TI does not recommend thermal reliefs in
this area.
- Use wide traces for the CBOOT
capacitor. Place CBOOT close to the device with short and
wide traces to the BOOT and SW pins. TI does not recommend thermal reliefs in
this area.
- Place the feedback divider as close as
possible to the FB pin of the device. If an external feedback divider is
used with the ADJ option, place RFBB, RFBT, and
CFF close to the device. The connections to FB and AGND must be
short and close to those pins on the device. The connection to VOUT
can be somewhat longer. However, this latter trace must not be routed near any
noise source (such as the SW node) that can capacitively couple into the
feedback path of the regulator.
- Use at least one ground plane in one of the
middle layers. This plane acts as a noise shield and also act as a heat
dissipation path.
- Connect the thermal pad to the ground
plane. The thermal pad (DAP) connection must be soldered down to the PCB
ground plane. This pad acts as a heat-sink connection and an electrical ground
connection for the regulator. The integrity of this solder connection has a
direct bearing on the total effective RθJA of the application. TI
does not recommend thermal reliefs in this area.
- Provide wide paths for VIN, VOUT, SW, and
PGND. Making these paths as wide and direct as possible reduces any
voltage drops on the input or output paths of the converter and maximizes
efficiency. TI does not recommend thermal reliefs in this area.
- Provide enough PCB area for proper
heat-sinking. As stated in Section 8.2.2.8, enough copper area must be used to make sure of a low
RθJA, commensurate with the maximum load current and ambient
temperature. The top and bottom PCB layers must be made with 2oz copper and no
less than one ounce. Use an array of heat-sinking vias to connect the thermal
pad (DAP) to the ground plane on the bottom PCB layer. If the PCB design uses
multiple copper layers (recommended), these thermal vias can also be connected
to the inner layer heat-spreading ground planes.
- Keep switch area small. Keep the copper
area connecting the SW pin to the inductor as short and wide as possible. At the
same time, the total area of this node must be minimized to help reduce radiated
EMI.
See the following PCB layout resources for additional important guidelines: