SNVSCP5C April 2025 – August 2026 TPS7H3024-SP , TPS7H3034-SP , TPS7H3124-SP , TPS7H3134-SP
PRODUCTION DATA
During steady state operation, the input voltage of the TPS7H3024 must be from 3V to 14V. A minimum bypass capacitance of 0.1μF is required between VIN and GND. The input bypass capacitors is recommended to be placed as close to the device as possible. The VIN slew rate must be controlled between 10V/μs to 1mV/μs for proper IC operation.
The voltage applied at VIN serves as the input for the internal regulator that generates the VLDO voltage, typically 3.29V. At input voltages less than 3.65, the VLDO regulator can be on dropout. The recommended capacitance for VLDO is 1μF of ceramic type. The VLDO can be loaded up to a maximum of 5mA.
Each device generates an internal 1.2V bandgap reference that is used throughout the various internal control logic blocks. This is the voltage present on the REFCAP pin during steady state operation. This voltage is divided down to produce the reference for the comparator inputs at:
A 470nF capacitor to GND is required at the REFCAP pin for proper electrical operation as well as to provide robust SET performance of the device.