SNVSCT9A October 2024 – February 2025 LM251772
PRODUCTION DATA
The 7 bit target address of this device is 0x6A if the ADDR/SLOPE pin I pulled to GND and 0x6B if the pin is connected to VCC2
Data transmission is initiated with a start bit from the controller as shown in the figure below . The start condition is recognized when the SDA line transitions from high to low during the high portion of the SCL signal. Upon reception of a start bit, the device will receive serial data on the SDA input and check for valid address and control information. If the target address bits are set for the device, then the device issues an acknowledge pulse and prepares the receive of register address and data. Data transmission is completed by either the reception of a stop condition or the reception of the data word sent to the device. A stop condition is recognized as a low to high transition of the SDA input during the high portion of the SCL signal. All other transitions of the SDA line must occur during the low portion of the SCL signal. An acknowledge is issued after the reception of valid address, sub-address and data words. The I 2 C interfaces will auto-sequence through register addresses, so that multiple data words can be sent for a given I 2 C transmission.
Figure 8-35 I
2 C START / STOP / ACKNOWLEDGE Protocol
Figure 8-36 I
2 C Data Transmission Timing
Figure 8-37 I 2 C Data
Transmission Timing for maximum rise/fall times.