This section describes the connectors, test
points, and jumpers on the EVM and how to properly connect, set up, and use the LM65635EVM
See Figure 2-3 for location of connectors and jumpers and typical setup.
VOUTOutput voltage of the converter.VOUT banana post. Apply load to this connector.
VOUTS
The VOUTS test point is used to monitor output voltage.
GNDS
Test point next to VOUTS test point.
This GNDS test point is use as the negative DMM connection for VOUT sensing.
VINInput voltage to the converter.VIN banana post. Apply input voltage to this connector.
VINS
The VINS test point is used to monitor input voltage.
GNDS
Test point next to VINS test point.
This GNDS test point is use as the negative DMM connection for VIN sensing.
GND
Ground of the converter
GND banana posts. Apply load ground and input voltage ground to these connectors. The
various GND test point are used as ground sense for input voltage and output voltage
measurements.
ENThe use of the EN jumper is self-explanatory. To supply an external signal to the EN input of the device, remove the EN jumper shunt and apply
the signal to the EN test point.
To use the external UVLO feature, populate Rent (R3) and Renb (R4) as desired and
remove the EN jumper shunt. Note that for accurate shutdown current measurement, these
resistors must be removed (if used) and the EN jumper shunt moved to "OFF".
RTThe RT jumper is used to select the switching frequency and is self explanatory.The default inductor on the EVM is designed for 2.2MHz operation. Other frequencies require a
different value of inductance.
To adjust the switching frequency, remove the RT jumper shunt and populate RT (R5)
with the desired value. See the LM656x5 data sheet for frequency vs. RT resistor
value.
MODEMODE jumper is used to select the operating mode of the device. With MODE in the AUTO position,
the device operates in automatic PFM/FPWM mode depending on load current. With the MODE
in the FPWM position, the device operates at fixed frequency for all load currents.The MODE pin is also the frequency synchronization input. To synchronize the device to an
external clock, remove the MODE jumper shunt and apply the clock to the MODE test
point.
Feed-back Connections
The EVM is set for a fixed 5V output, with Rfbt2 (R7), 0Ω, populated. To set the
output voltage to 3.3V, remove Rfbt2 (R7) and populate Rfbb (R10) with a 0Ω
resistor.
To use the adjustable output voltage option, populate Rfbt (R9) and Rfbb (R10) with
the appropriate value resistors. Rinj (R8) must also be populated with a 10Ω to 50Ω
resistor. The reference voltage is 0.8V. See the LM656x5-Q1 High Performance Power Converter, 3V
to 65V, Pin-Compatible, 2.5A/3.5A/4.5A, Automotive, Low EMI Synchronous Buck
Converter data sheet for appropriate values of feed-back resistors.
When using the adjustable output voltage mode, a Bode plot can be taken using the Rinj
(R8) resistor. This resistor becomes the injection point for the frequency response
analyzer, allowing the loop frequency response to be taken in the usual way. In the
fixed output voltage mode, a Bode plot can not be taken.
PGOODThe PGOOD test point is used to monitor the power-good indicator. This flag indicates whether
the output voltage has reached the regulation level. PGOOD is an open-drain output that
is tied to VOUT through a 100kΩ, resistor, Rpg (R1).
VCC
VCC Test point
The VCC pin is the output of the internal LDO. The VCC voltage is typically 3.3V.
This point can be used for logic inputs and/or pull-up. Do not connect to external
loads.
BIAS
Auxiliary input to LDO
Connected to VOUT through 0Ω Rbias (R11) on EVM. To change the input supply of the
LDO, remove Rbias (R11) and connect external supply to BIAS pin, or ground BIAS pin as
required. Populate Cbias (C11) when using an external bias supply. See the LM656x5
data sheet for more information.
Bode Plot
When using the adjustable output voltage mode, a bode plot can be taken using the
connection shown in Figure 2-4. Rinj (R8) must be populated.
EMI Filter
The EMI filter is not populated on the EVM. To test the EMI filter, components L2, C1
and C2 must be populated, while R12 must be removed. Typical values of these components
are given in Section 4.3.