SPMA082 August 2021 TM4C1230C3PM , TM4C1230D5PM , TM4C1230E6PM , TM4C1230H6PM , TM4C1231C3PM , TM4C1231D5PM , TM4C1231D5PZ , TM4C1231E6PM , TM4C1231E6PZ , TM4C1231H6PGE , TM4C1231H6PM , TM4C1231H6PZ , TM4C1232C3PM , TM4C1232D5PM , TM4C1232E6PM , TM4C1232H6PM , TM4C1233C3PM , TM4C1233D5PM , TM4C1233D5PZ , TM4C1233E6PM , TM4C1233E6PZ , TM4C1233H6PGE , TM4C1233H6PM , TM4C1233H6PZ , TM4C1236D5PM , TM4C1236E6PM , TM4C1236H6PM , TM4C1237D5PM , TM4C1237D5PZ , TM4C1237E6PM , TM4C1237E6PZ , TM4C1237H6PGE , TM4C1237H6PM , TM4C1237H6PZ , TM4C123AE6PM , TM4C123AH6PM , TM4C123BE6PM , TM4C123BE6PZ , TM4C123BH6PGE , TM4C123BH6PM , TM4C123BH6PZ , TM4C123BH6ZRB , TM4C123FE6PM , TM4C123FH6PM , TM4C123GE6PM , TM4C123GE6PZ , TM4C123GH6PGE , TM4C123GH6PM , TM4C123GH6PZ , TM4C123GH6ZRB , TM4C1290NCPDT , TM4C1290NCZAD , TM4C1292NCPDT , TM4C1292NCZAD , TM4C1294KCPDT , TM4C1294NCPDT , TM4C1294NCZAD , TM4C1297NCZAD , TM4C1299KCZAD , TM4C1299NCZAD , TM4C129CNCPDT , TM4C129CNCZAD , TM4C129DNCPDT , TM4C129DNCZAD , TM4C129EKCPDT , TM4C129ENCPDT , TM4C129ENCZAD , TM4C129LNCZAD , TM4C129XKCZAD , TM4C129XNCZAD
Western languages such as English uses letters to compose words. The number of letters or characters in Western languages is generally small and can be easily encoded using 7-bit character encoding scheme such as ASCII. However, languages such as Chinese consists of tens of thousands of characters. A typical font set for Chinese would have taken up enormous amount of memory in the range of megabytes. Certainly, this is not practical for embedded applications.
An application requiring Chinese language may only need to use a small subset of the Chinese characters. For example, if an application only needs to use 100 unique Chinese characters and if these 100 characters are known ahead of time then the programmer can create a custom font that only supports these 100 characters which will result in a small memory footprint. This is the purpose of creating custom fonts for non-Latin languages.
Examine the code snippet of a simple example shown in Figure 5-1 to demonstrate the effect of using custom font. The full source code can be found in Section A.
For how to generate this custom font: see Section 5.1.
Figure 5-1 Custom Font Demonstration
Figure 5-2 Custom Font Display
Figure 5-3 Unicode Converter