This document uses the following conventions.
- Hexadecimal numbers are shown with the suffix h
or the prefix 0x. For example, the following number
is 40 hexadecimal (decimal 64): 40h or 0x40.
- Registers in this document are shown in figures
and described in tables.
- Byte convention for N
bytes is 0 through (N-1) bytes.
- Bit convention for N
bits is 0 through (N-1) bits.
- Each register figure shows a rectangle divided
into fields that represent the fields of the
register. Each field is labeled with the bit name,
the beginning and ending bit numbers above, and
the read/write properties with default reset value
below. A legend explains the notation used for the
properties.
- Reserved bits in a
register figure can have one of multiple meanings:
- Not
implemented on the device
- Reserved for
future device expansion
- Reserved for
TI testing
- Reserved
configurations of the device that are not supported
- Writing nondefault values to the Reserved bits
can cause unexpected behavior and are to be
avoided.