SPMU378A April 2026 – August 2026 TPS26750A
| Description | The 'GSrC' Task instructs PD Controller to issue a Get_Source_Cap message to the Port Partner device at the first opportunity while maintaining policy engine compliance. |
|---|---|
| INPUT DATAX | None |
| OUTPUT DATAX | Byte 1: Standard Task Return Code. See also Table 4-1. |
| Task Completion | The 'GSrC' Task completes either when the Source Capabilities message is received or the Task otherwise fails. The 'GSrC' Task shall be considered rejected if:
|
| Side Effects | When the 'GSrC' Task completes successfully the RX_SOURCE_CAPS register (0x30) will have been updated. |
| Additional Information | None |