SPRABN2A March   2019  – December 2019 AM3352 , AM3354 , AM3356 , AM3357 , AM3358 , AM3358-EP , AM3359

 

  1.   AM335x Schematic Checklist
    1.     Trademarks
    2. 1 Introduction
    3. 2 Recommendations Specific to AM335x
      1. 2.1  Unused Signals
      2. 2.2  SYSBOOT Configuration and Required Termination
      3. 2.3  System Issues
        1. 2.3.1 Pinmux
        2. 2.3.2 Pullups
        3. 2.3.3 General Debug
        4. 2.3.4 Warm Reset
        5. 2.3.5 Peripheral Clocking
      4. 2.4  Low-Power Considerations
      5. 2.5  Clocking
      6. 2.6  General DDR Guidelines
        1. 2.6.1 DDR2
        2. 2.6.2 DDR3
      7. 2.7  MultiMedia Card/ (MMC)
      8. 2.8  Inter-Integrated Circuit (I2C)
      9. 2.9  LCD
      10. 2.10 Power
      11. 2.11 Touchscreen
        1. 2.11.1 If ADC/Touchscreen is not Used
      12. 2.12 USB
        1. 2.12.1 If USB0 or USB1 is not Used
      13. 2.13 External Interrupt (EXTINTn)
      14. 2.14 Ethernet
    4. 3 References
  2.   Revision History

Pullups

  • Ensure all pullups connected to AM335x are pulled up to the correct I/O voltage to avoid any leakage between the I/O rails of AM335x. Each terminal has an associated voltage used to power its I/O cell. This can be found in the AM335x data sheet, in the Ball Characteristics table under the "ZCE Power/ ZCZ Power" column.
    • For example, if you want to pull up terminal SPI0_CS0 in any mux mode (gpio0_5, i2c1_scl, and so forth), pull up the signal to VDDSHV6.