SPRACN3 September   2019 66AK2E05 , 66AK2H06 , 66AK2H12 , 66AK2H14 , 66AK2L06 , AM5K2E02 , AM5K2E04

 

  1.   Using ARM ROM Bootloader on Keystone II Devices
    1.     Trademarks
    2. 1  Keystone2 Boot loader Overview
    3. 2  Boot Examples Package Download
    4. 3  Software Dependencies
    5. 4  Supported Hardware
    6. 5  Software Features
    7. 6  Directory Structure
    8. 7  Building the Examples
    9. 8  Description of the Examples
      1. 8.1 Single Stage Boot Examples
      2. 8.2 Multi-Stage Boot Example
      3. 8.3 Boot Media-Specific Details
        1. 8.3.1 SPI Boot Example
        2. 8.3.2 I2C Boot Examples
        3. 8.3.3 NAND Examples
        4. 8.3.4 UART Boot Examples
        5. 8.3.5 Ethernet boot examples
        6. 8.3.6 K2E Ethernet Boot Errata Workaround
      4. 8.4 Flashing and Running Boot Examples
        1. 8.4.1 Dip Switch Settings
        2. 8.4.2 Running I2C EEPROM example
        3. 8.4.3 Running SPI NOR Example
        4. 8.4.4 Running NAND Example
        5. 8.4.5 Running UART Example
        6. 8.4.6 Running Ethernet Examples
    10. 9  Boot Utilities
    11. 10 Frequently Asked Questions (FAQ)
    12. 11 References

Single Stage Boot Examples

Single stage boot examples demonstrate booting the K2 devices directly from the boot media specified by the boot mode pins using the default settings specified by the boot parameter loaded by the BootROM. For default boot parameter settings used by the bootROM, see the device-specific data manual. The sample application is designed to wake up the secondary Arm core upon boot and then initializes the UART to print message when each core wakes up. Each Arm core will send a message over UART: "Core n standing by..." where n is the Arm core number.