SPRACV3 December 2020 AM6412 , AM6422 , AM6442
The Torrent16FFC TX AMI parameters are listed in Figure 2-8. In Cadence SystemSI, clicking on a parameter value opens the AMI Parameter Editor where you can change the value. The preset values can be chosen at “Default_preset_Value”.
Figure 2-8 Tx Algorithmic Model
ParametersTable 2-3 provides a description of the Torrent16FFC TX AMI parameters:
| Parameter | Description |
|---|---|
| Deemphasis_code | You can set the TX De-emphasis tap coefficients. The drive strength in decibels is set according to the De- emphasis code that is selected. For example, code P1 equates to drive strength of -3.5db. The default value is P1. |
| Deemphasis_tap_definition<tap values> | For more information, see Table 2-4. |
| Vmargin | For more information, see Table 2-5. |
| Swing_mode | It can have following modes :
|
| self_adapt_ffe<TRUE|FALSE> | A value of TRUE results in the best CTLE curve being selected during simulation to find the most optimized FFE taps at Tx for the current channel. The default value of this parameter is ‘TRUE’. |
| Pre_cursor_tap, main_tap, post_cursor_tap | C-1, C0 & C+1 can be specified.
C0,max (FS) value is 46. C0,max = 46, C0,min = 26 C-1,max = 0, C-1,min = -9 C+1,max = 0, C+1,min = -17 Default values are: C0 = 31, C-1 = -3, C+1 = -12 |