SPRADG1A February 2024 – October 2026 AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM625SIP
Low Power Mode test results for Deep Sleep measurements demonstrated a range of results from 25-34mW. This is expected for several reasons: First, the VDD_DDR4 (and LPDDR4) rail sources power to both the AM62x SoC DDR IO rails, as well as the DDR IC power-supply rails. Per the table found in Starter Kit EVM Rails, there will be power consumed on the DDR rail by the DRAM IC. More information can be found about the expected power consumed by the Micron DDR IC in their device specific App Notes. Often the values needed to evaluate are ‘IDD6N, Self Refresh Current’, for LPDDR4 and DDR4 memory types.
An additional reason for varying power measurements in the Deep Sleep modes is due to the IO power supply rails are not yet optimized with internal Pull Ups and Pull Downs for Deep Sleep modes, for each AM62x variant board type. The default resistor configuration does not follow recommendations from the legacy Sitara AM335x Low Power Design Guide.