Before posting an OSPI/FLASH related
question on the TI
E2E™ forum, it is helpful if the following queries are addressed:
- Which TI processor is used?
- What is the MCU+ SDK version used?
- Is the testing done on a custom board or a TI EVM?
- Name the custom flash part and attach the
datasheet.
- Are the values in SysConfig verified with the Flash
datasheet?
- Share the failure logs or the point of failure by following the
debugging guide here.
- Point to a specific section from this application note which
resembles close to the failure observed on the test board.