SPRADS5 December 2025 AM625 , AM62A7 , AM62D-Q1 , AM62P , AM6442
SysConfig is a configuration tool designed to simplify hardware and software configuration challenges to accelerate software development.
In MCU+SDK, for a custom flash, the section which needs modification is shown in Figure 4-1.
Figure 4-1 SysConfig GUI Showing FLASH and OSPI
SectionsTo obtain the custom flash configuration values, follow the guide here. This guide currently works for Serial NOR flash. For Serial NAND flash, the configuration values must be obtained from the datasheet of the flash.
Upon obtaining the values, the FLASH section can be filled up with the obtained values. These values can be filled up manually or uploaded in a json format. Verify the values obtained by running the OSPI Flash Diagnostics example with the values mentioned in the flash datasheet. The following sections show the various parameters in FLASH and OSPI sections.