SPRADT1 May 2025 AWR1642 , AWR1843 , AWR2944 , AWR6843 , AWRL1432
The HWA and the mmWave radar chip processor work in parallel, as shown in the block diagram below. The HWA connects to other systems via a 128-bit bus (64-bit bus for HWA version 1.2). HWA2.1 of the AWR2944, for example, contains an accelerator engine and eight 16KB memories, which are used to provide input and output data to the accelerator's computation engine. The HWA does not have direct access to memory units external to the accelerator. Data can only be transferred to or from the HWA memory via DMA or the processor to facilitate data exchange. The internal memory is divided into separate 16KB units, allowing simultaneous reads and writes via DMA or the processor, and uses a ping-pong buffering mechanism to process data. The HWA internal access bus is 128 bits wide, allowing a throughput of 128 bits per clock cycle.
It is important to note that any 16KB HWA local memory unit can serve as the source address for the accelerator engine's input data, and any of them can serve as the destination address for the output data, with one important limitation: The source and destination addresses cannot be the same 16KB unit. In other words, the same memory unit cannot be used for overwrite operations during a single computation. It is also important to note that the accelerator's local memories do not mandatorily require ping-pong mode. If the application scenario demands, two or four memory units can be combined into a larger 32KB or 64KB input and output unit. The HWA internal access to these memories starts at address 0x0000.
Figure 2-1 Hardware Accelerator System