SPRADT1 May 2025 AWR1642 , AWR1843 , AWR2944 , AWR6843 , AWRL1432
In the DopplerProcDDMA processing flow, the HWA and DSP/MCU must work together for data processing, which is divided into four primary stages. The flow chart and detailed description are as follows.
Figure 4-2 Doppler DDMA FlowWhen the DPU is initiated, if the Range DPU applies data compression, the HWA is required for decompression. To improve HWA execution efficiency and reduce parameter set reconfiguration time, the Doppler DPU typically reads in all eight range bins across all Chirps at once for data decompression. For example, assuming there are 96 Chirps and each block has a rangeBinsPerBlock of 2, in EGE mode, the size of a single read-in block is 96 * (sizeOfCompressedBlock). In BFP mode, because the data of each receive antenna is compressed individually, the data volume in the decompression stage must be multiplied by the number of receive antennas, i.e., 96 * (sizeOfCompressedBlock) * RxAnt.
After decompression, the Doppler DPU invokes the HWA to perform windowing, Doppler FFT, and DDMA demodulation on the decompressed data. On radar processors without a DSP, the HWA continues to perform DDMA demodulation using the summation and maximum value functions in its Statistics module after completing the FFT. On processors with a DSP, while DDMA demodulation is performed by the DSP core, the HWA continues with the Doppler FFT on the next range bin.
After the Doppler FFT and DDMA demodulation, the HWA continues with the horizontal angle (Azimuth) calculation.
The CFAR engine of the HWA performs CFAROS detection in the Doppler dimension, and then the Local Maxima engine performs detection on the two-dimensional speed-azimuth plot. The results of the two detections are then combined. Because the detection proceeds from near range to far range gradually, in order to prevent an excessive number of near-range objects from restricting the radar detection range due to memory constraint, the number of detection objects per range bin is limited by the macros LIMIT_DETECTED_OBJS_PER_RANGEBIN and MAX_NUM_OBJ_PER_RANGE_BIN.