SPRUI64F May 2017 – October 2025
The system view of the AM572x IDK EVM consists of the main board and the camera board. There is also an optional LCD panel and touch screen assembly that can be attached to the AM572x IDK EVM.
The top and the bottom views of the AM572x IDK EVM are provided in Figure 2-1 and Figure 2-2, respectively.
The top and the bottom views of the AM572x IDK EVM with the optional LCD display assembly attached are provided in Figure 2-3 and Figure 2-4, respectively.
Figure 2-1 AM572x IDK EVM - Top View
Figure 2-2 AM572x IDK EVM - Bottom View
Figure 2-3 AM572x IDK EVM with LCD Display Assembly Attached - Top View
Figure 2-4 AM572x IDK EVM with LCD Display Assembly Attached - Bottom View