SPRUIX1B October 2022 – April 2024 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137
SYS_ERR consolidate several sources of interrupts (see Figure 3-3). These sources set the respective bit in the SYS_ERR_INT_FLG register. Any set bit in the SYS_ERR_INT_FLG register also sets the global interrupt (GINT) bit. The GINT bit has to be cleared before any SYS_ERR interrupt is generated. If the GINT bit is cleared with the source flags still set, another SYS_ERR interrupt is fired; therefore, it is recommended to clear the source flags before clearing the GINT bit.
Figure 3-3 System Error