SPRUIX1B October 2022 – April 2024 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137
Flash memory is typically used to store application code. During code execution, instructions are fetched from contiguous memory addresses, except when a discontinuity occurs. Usually, the portion of the code that resides in contiguous address locations makes up the majority of the application code, and is referred to as linear code. To improve the performance of linear code execution, a Flash prefetch mechanism has been implemented. Figure 6-2 illustrates how this mode functions.
The prefetch mechanism does a
look-ahead prefetch on linear address increments, starting from the address of the
last instruction fetch. The Flash prefetch mechanism is disabled by default. To
enable prefetch mode, set the PREFETCH_EN bit in the FRD_INTF_CTRL register, or call
the Flash_enablePrefetch() driverlib function.
Each instruction fetch from the Flash or OTP reads out 128 bits. The starting address of the access from Flash is automatically aligned to a 128-bit boundary, such that the instruction location is within the 128 bits to be fetched. When Flash prefetch mode is enabled, the 128 bits read from the instruction fetch are stored in a 128-bit wide by 2-level deep instruction prefetch buffer. The contents of this prefetch buffer are then sent to the CPU for processing as required.
Up to four 32-bit or eight 16-bit instructions can reside within a single 128-bit access. The majority of C28x instructions are 16 bits, so for every 128-bit instruction fetch from the Flash bank there are up to eight instructions in the prefetch buffer ready to process through the CPU. During the time to process these instructions, the Flash prefetch mechanism automatically initiates another access to the Flash bank to prefetch the next 128 bits. The Flash prefetch mechanism works in the background to keep the instruction prefetch buffers as full as possible. Using this technique, the overall efficiency of sequential code execution from Flash or OTP is improved significantly.
Figure 6-2 Flash Prefetch ModeThe Flash prefetch is aborted only when there is a code discontinuity caused by executing an instruction such as a branch, function call, or loop. When this occurs, the prefetch mechanism is aborted, and the contents of the prefetch buffer are flushed. There are two possible scenarios when this occurs:
Note that the prefetch mechanism gets bypassed when RWAIT is configured as zero.