SPRUJ63B September   2022  – November 2025

 

  1.   1
  2.   Trademarks
  3. 1Introduction
    1. 1.1 EVM Revisions and Assembly Variants
    2. 1.2 Inside the Box
  4. 2Important Usage Notes
    1. 2.1 Power-On Usage Note
    2. 2.2 EMC, EMI, and ESD Compliance
  5. 3System Description
    1. 3.1 Key Features
    2. 3.2 Functional Block Diagram
    3. 3.3 Power-On/Off Procedures
      1. 3.3.1 Power-On Procedure
      2. 3.3.2 Power-Off Procedure
    4. 3.4 Peripheral and Major Component Description
      1. 3.4.1  Clocking
        1. 3.4.1.1 Ethernet PHY Clock
        2. 3.4.1.2 AM64x/AM243x Clock
        3. 3.4.1.3 PCIe Clock
      2. 3.4.2  Reset
      3. 3.4.3  Power
        1. 3.4.3.1 Power Input
        2. 3.4.3.2 Reverse Polarity Protection
        3. 3.4.3.3 Current Monitoring
        4. 3.4.3.4 Power Supply
        5. 3.4.3.5 Power Sequencing
        6. 3.4.3.6 AM64x/AM243x Power
      4. 3.4.4  Configuration
        1. 3.4.4.1 Boot Modes
      5. 3.4.5  JTAG
      6. 3.4.6  Test Automation
      7. 3.4.7  UART Interfaces
      8. 3.4.8  Memory Interfaces
        1. 3.4.8.1 DDR4 Interface
        2. 3.4.8.2 MMC Interfaces
          1. 3.4.8.2.1 Micro SD Interface
          2. 3.4.8.2.2 eMMC Interface
        3. 3.4.8.3 OSPI Interface
        4. 3.4.8.4 SPI EEPROM Interface
        5. 3.4.8.5 Board ID EEPROM Interface
      9. 3.4.9  Ethernet Interface
        1. 3.4.9.1 DP83867 PHY Default Configuration
        2. 3.4.9.2 DP83869 PHY Default Configuration
        3. 3.4.9.3 Ethernet LED
      10. 3.4.10 Display Interface
      11. 3.4.11 USB 2.0 Interface
      12. 3.4.12 PCIe Interface
      13. 3.4.13 High Speed Expansion Interface
      14. 3.4.14 CAN Interface
      15. 3.4.15 Interrupt
      16. 3.4.16 ADC Interface
      17. 3.4.17 Safety Connector
      18. 3.4.18 SPI Interfaces
      19. 3.4.19 I2C Interfaces
      20. 3.4.20 FSI Interface
  6. 4Known Issues and Modifications
    1. 4.1 Issue 1 - Embedded XDS110 Connection to AM64x Target in CCS
    2. 4.2 Issue 2 - DC Barrel Jack Warning when Hot-Plugging
    3. 4.3 Issue 3 - uSD Card Boot Not Working
    4. 4.4 Issue 4 - Damage LM5140 after Hot Plug DC Jack
  7. 5References
  8. 6Revision History

DP83869 PHY Default Configuration

The DP83869 PHY uses four level configurations for I/O, RX_D0 and RX_D1 pins and two-level configurations for all other pins. The four level strap pins based on resistor strapping generates four distinct voltages ranges. The resistors are connected to the RX data pins, which are normally driven by the PHY and are inputs to the AM64x/AM243x. The voltage range for each mode is shown below:

Mode 0 - 0 V to 0.3069 V

Mode 1 – 0.4488 V to 0.6072 V

Mode 2 – 0.7227 V to 0.924 V

Mode 3 – 1.98 V to 2.9304 V

The two level strap pins based on resistor strapping generates two distinct voltage ranges. The resistors are connected to the LED pins. Because the LED output pins are also used as straps, the external components required for strapping and LED usage must be considered to avoid contention. Specifically, this can be an issue when the LED outputs are used to drive LED directly. The voltage range for each mode is shown below:

Mode 0 - 0 V to 0.594 V

Mode 1 – 1.65 V to 2.904 V

DP83869 device includes internal pull-down resistor. The value of the external pull resistors is selected to provide voltage at the pins of the AM64x/AM243x as close to ground or 3.3 V as possible. The strapping is shown in Figure 3-22 and the strap values are given in Table 3-20.

Address strapping is provided for ICSSG1 PHY to set address of 00011 (03h) and ICSSG2 PHY to set address of 01111 (0Fh) using the strap resistors. Footprint for both pull up and pull down is provided on all the strapping pins.

Table 3-19 Default Strap Setting of CPSW Ethernet PHY
Strap SettingPin NameStrap FunctionMode for PRG0_PRU1,
PRG0_PRU0,
PRG1_PRU1,
PRG1_PRU0
Value of Strap Function for PRG0 and PRG1Description
PHY AddressRX_D2PHY_AD310PHY Address: 0000
PHY_AD210
RX_D0PHY_AD110
PHY_AD010
Auto NegotiationRX_DV/RX_CTRLAuto-neg30Auto neg Disable=0
Modes of OperationLED_2RGMII Clock Skew TX[1]10RGMII TX Clock Skew is set to 2 ns
RGMII Clock Skew TX[0]10
LED_1RGMII Clock Skew TX[2]10
ANEG_SEL10advertise ability of 10/100/1000
LED_0Mirror Enable10Mirror Enable Disabled
GPIO_1RGMII Clock Skew RX[2]10RGMII RX Clock Skew is set to 2 ns
RGMII clock Skew TX[1]10
GPIO_0RGMII clock Skew RX[0]10
Table 3-20 Default Strap Setting of ICSSG Ethernet PHYs
Strap SettingPin NameStrap FunctionMode for PRG1_RGMII2 (ICSSG1)Value of Strap Function for PRG1_RGMII2 (ICSSG1)Mode for PRG1_RGMII1 (ICSSG2)Value of Strap Function for PRG1_RGMII1 (ICSSG2)Description
PHY AddressRX_D1PHY_AD33131ICSSG1 PHY Address: 00011
PHY_AD23131
RX_D0PHY_AD10031ICSSG2PHY Address: 01111
PHY_AD00031
Modes of OperationRX_CNTLMirror Enable0000Mirror Enable Disabled
LED_2ANEGSEL_10000Auto-negotiation, 10/100/1000 advertised, Auto-MDI-X
LED_1ANEGSEL_00000
LED_0ANEG_DIS0000
JTAG_TDO/GPIO_1OPMODE_00000RGMII to Copper (1000BaseT/100Base-TX/10Base-Te)

The PHY devices include integrated MDI termination resistors, so external termination is not provided.

Interrupt: The interrupt from two ICSSG PHYs from PRG1 domain are tied together and is connected to EXTINTN pin of the AM64x/AM243x. An option for connecting the interrupt from CPSW PHY to the PRG1 ICSSG Interrupt pins is also provided.

Three configurable LED pins and a GPIO of Ethernet PHY are used to indicate link status. Several functions can be multiplexed onto the LEDs for different modes of operation. The LED operation mode can be selected using the LEDCR1 register address 0x0018 on the DP83867 device and LEDS_CFG1 register address 0x0018 on the DP83869 device. The default configuration are as follows.

LED0: By default, this pin indicates that link is established. Additional functionality is configurable via LEDCR1[3:0] register bits in the DP83867 device and LEDS_CFG1[3:0] register bits in the DP83869 device. LDE0 is not used in the CPSW PHY (DP83867), this is also a strap pin which is used to set mirror enable. Since these features are not required the strapping for the LED0 is not provided. In the DP83869 ICSSG PHY the LED0 is connected to PRG1_PRU1_GPO8 and PRG1_PRU0_GPO8 of SoC for link status. This pin is also a strap pin which is having internal pulldown resistor to set Auto Negotiation Disable option in the DP83869 device. The default condition is to auto negotiate and advertise link as 10/100/1000Mbps

LED_1: By default, this pin indicates that 1000BASE-T link is established. This setting can be changed to Auto negotiate to 10/100Mbps using the strap resistors. Additional functionality is configurable via LEDCR1[7:4] register bits in the DP83867 device and LEDS_CFG1[7:4] register bits in the DP83869 device. LED_1 is a also an strap pin, which is having internal pulldown resistor to set RGMII TX Clock Skew in the DP83867 device and to select Auto Negotiation mode in the DP83869 device. Since this pin is set to active on both the devices, this results in dim LED lighting when LED is driven directly. Therefore, a MOSFET is used to drive LED, as shown in Figure 3-24.

LED_2: By default, this pin indicates receive or transmit activity. Additional functionality is configurable via LEDCR1[11:18] register bits in the DP83867 device and LEDS_CFG1[11:18] register bits in the DP83869 device. LED_2 is also a strap pin, which is having internal pulldown resistor to set RGMII TX Clock Skew in the DP83867 device and to select Auto Negotiation mode in the DP83869 device. The default condition is to auto negotiate and advertise link as 10/100/1000Mbps, this can be changed using the strap resistors provided. The pull up resistor used for strap setting results in dim LED lighting when LED is driven directly. So a MOSFET is used to drive LED .

GPIO1: In the DP83867 PHY, the GPIO can be configured to function as LED3 through GPIO Mux Control Register 1 (GPIO_MUX_CTRL1) and the LED configuration can be set by programming LEDCR1 register. This is also a strap pin which is used to set fast link drop (FDP), and is currently disabled. In the DP83869 PHY, the GPIO can be configured to function as LED_GPIO(3) through GPIO Mux Control Register (GPIO_MUX_CTRL) and the LED configuration can be set by programming LEDS_CFG1 register. This is also a strap pin which is used to select RGMII to copper mode of operation on startup. This can be changed to MII mode using the MDC &MDIO pin to update the GEN_CFG1 register – 0x9 (gigabit Ethernet advertising must be disabled when using MII mode as the PHY does not link up at 1000Mbps speed)

RJ45 Connector LED Indication -CPSW (DP83867):

LED1 and GPIO1 is connected to dual LEDs of RJ45 to indicate 10/100 or 1000 MHz link. Orange LED indicates 10/100 speed and Green LED is to indicate 1000 MHz speed.

LED2 is connected to RJ45 LED (Yellow) to indicate transmit/receive activity.

RJ45 Connector LED Indication -ICSSG (DP83869):

LED1 is connected to RJ45 LED (Green) to indicate 1000 MHz speed.

LED2 is connected to RJ45 LED (Yellow) to indicate transmit/receive activity.

TMDS243EVM TMDS64EVM AM64x/AM243xEthernet Interfaces - CPSW Ethernet Strap SettingsFigure 3-21 AM64x/AM243xEthernet Interfaces - CPSW Ethernet Strap Settings
TMDS243EVM TMDS64EVM AM64x/AM243x Ethernet Interfaces - ICSSG1 Ethernet Strap SettingsFigure 3-22 AM64x/AM243x Ethernet Interfaces - ICSSG1 Ethernet Strap Settings
TMDS243EVM TMDS64EVM AM64x/AM243x Ethernet Interfaces - ICSSG2 Ethernet Strap SettingsFigure 3-23 AM64x/AM243x Ethernet Interfaces - ICSSG2 Ethernet Strap Settings
Note: Resistors that are highlighted by red color box are DNI components.