SPRZ488G March   2022  – September 2026 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1

 

  1.   1
  2. 1Usage Notes and Advisories Matrices
  3. 2Silicon Usage Notes
    1.     i2324
    2.     i2348
    3.     i2364
    4.     i2508
  4. 3Silicon Advisories
    1.     i2310
    2.     i2311
    3.     i2313
    4.     i2329
    5.     i2345
    6.     i2346
    7.     i2347
    8.     i2349
    9.     i2350
    10.     i2352
    11.     i2353
    12.     i2354
    13.     i2355
    14.     i2356
    15.     i2357
    16.     i2358
    17.     i2359
    18.     i2374
    19.     i2375
    20.     i2386
    21.     i2392
    22.     i2393
    23.     i2394
    24.     i2395
    25.     i2401
    26.     i2402
    27.     i2403
    28.     i2404
    29.     i2405
    30.     i2427
    31.     i2428
    32.     i2433
    33.     i2438
    34.     i2439
    35.     i2488
    36.     i2499
    37.     i2500
    38.     i2502
    39.     i2503
  5.   Trademarks
  6. 4Revision History

i2500

LIN Module Fails to Wake Up When Using 0xF0 as Wake-Up Key

Details:

Using the wake-up key 0xF0 to wake up the LIN module causes the LIN state machine to enter a deadlock state. This renders 0xF0 unusable as a wake-up key for this module.

Workaround(s):

Instead of sending the 0xF0 wake-up signal:

Transmit a LIN header with an unused identifier (such as the reserved identifier 0x3E or any other identifier not used in your LIN network)

The break field contained within this header will:

  • Serve as a valid wake-up command to other LIN nodes on the network
  • Successfully clear the internal LIN POWERDOWN bit in the module