SPRZ491E December 2020 – December 2024 DRA821U , DRA821U-Q1
RAT: Error Interrupt Triggered Even When Error Logging Disable Is Set
If the RAT error logging is programmed to disable logging and enable interrupts, then an error will incorrectly trigger an interrupt but the error log registers will correctly not be updated. The error interrupt should not have been generated.
If the RAT error logging is disabled, then the error interrupt should also be disabled by software.