SPRZ491E December 2020 – December 2024 DRA821U , DRA821U-Q1
Boot: When disabling deskew calibration, ROM does not check if deskew calibration was enabled
If PLL Deskew calibration is being disabled, the ROM driver code intends to check if deskew calibration is enabled and if lock has failed. However the current code has an assignment in an if condition. As a result, it does not check if deskew calibration is enabled before clearing the config bit. There is no functional issue.
None