SPRZ576A November   2024  – April 2025 AM2612

 

  1.   1
  2.   Abstract
  3. 1Usage Notes and Advisories Matrices
  4. 2Silicon Revision 1.0 Usage Notes and Advisories
    1. 2.1 Silicon Revision 1.0 Usage Notes
      1.      i2324
    2. 2.2 Silicon Revision 1.0 Advisories
      1.      i2189
      2.      i2310
      3.      i2311
      4.      i2345
      5.      i2351
      6.      i2352
      7.      i2353
      8.      i2354
      9.      i2356
      10.      i2357
      11.      i2358
      12.      i2359
      13.      i2374
      14.      i2383
      15.      i2411
      16.      i2412
      17.      i2427
      18.      i2428
      19.      i2433
      20.      i2439
      21.      i2440
      22.      i2479
      23.      i2480
  5. 3Trademarks
  6. 4Revision History

i2374

PBIST fails if clock frequency of R5SS_CORE_CLK is not same as R5FSS_CLK_SELECTED frequency

Details

The R5SS memories receive the R5SS CPU clock “R5SS_CORE_CLK” which is derived from R5SS_CLOCK_SELECTED root clock using programmable divider. When R5SS memories are tested using PBIST controller, the PBIST controller receives R5SS_CLOCK_SELECTED root clock. PBIST operation fails if different frequencies are chosen for the two clocks.

Workaround

For PBIST to work with R5SS memories the frequency of both clocks need to be same. If application usage requires R5SS_CORE_CLK to be a divided frequency of R5SS_CLOCK_SELECTED, then during PBIST operation of R5SS memories, the application shall ensure the R5SS_CORE_CLK is configured to same frequency as R5SS_CLOCK_SELECTED.