SPVA024A June 2025 – October 2026 ADC810-Q1
PRODUCTION DATA
The ADC810-Q1 features a programmable digital comparator that can issue an alert on the ALERT/RDY pin. The COMP_MODE bit in the ADC Configuration register configures the comparator as either a traditional comparator or a window comparator. In traditional comparator mode, the ALERT/RDY pin asserts (active low by default) when conversion data exceeds the limit set in the high-threshold register (High_thresh). The comparator then deasserts only when the conversion data falls below the limit set in the low-threshold register (Low_thresh). In window comparator mode, the ALERT/RDY pin asserts when the conversion data exceed the High_thresh register or fall below the Low_thresh register value.
In either window or traditional comparator mode, the comparator can be configured to latch after being asserted by the COMP_LAT bit in the ADC Configuration register. This setting causes the assertion to remain even if the input signal is not beyond the bounds of the threshold registers. This latched assertion can only be cleared by reading the ADC Conversion register. The ALERT/RDY pin can be configured as active high or active low by the COMP_POL bit in the ADC Configuration register. Operational diagrams for both the comparator modes are shown in Figure 6-3.
The comparator can also be configured to activate the ALERT/RDY pin only after a set number of successive readings exceed the threshold values set in the threshold registers (High_thresh and Low_thresh). The COMP_QUE[1:0] bits in the ADC Configuration register configures the comparator to wait for one, two, or four readings beyond the threshold before activating the ALERT/RDY pin. The COMP_QUE[1:0] bits can also disable the comparator function, and put the ALERT/RDY pin into high-impedance.