STDA015 February 2026 DRV8163-Q1 , DRV8263-Q1 , LM61495-Q1 , LM70880-Q1 , LM74500-Q1 , LMR36503-Q1 , MCF8329A-Q1 , TLIN4029A-Q1
The wiper system, when powered by the 48V rail, uses a rotary motor, either DC brushed or brushless (BLDC), to actuate the wiper mechanism. The driver controls the speed of the motor or drives to the park position based on user settings and optional rain sensor input. Motor current and motion information can be fed back to the MCU for precise control.
Typically front wipers have two speeds, as well as intermittent operation. If the motor is brushed type, it often has two windings, one for each speed. Newer designs may use 48V brushless motors which can be more efficient and long-lived. The speed of a brushless motor can be controlled by adjusting the phasing of the electrically commutated drive voltages.
An example block diagram for a 48V wiper module using a BLDC motor is shown in Example 48V Window Lift Block Diagram.
Figure 2-3 Example 48V Windshield Wiper
Block DiagramThe MCF8329A-Q1 BLDC gate driver shown in this example includes a 50 mA 3.3V regulator able to supply up to 50mA to external circuits. This regulator is disabled when the chip is in low-power sleep mode, but if the 48V supply to the wiper ECU is switched by an upstream Zone module or power distribution box, the regulator integrated in the MCF8329A-Q1 can be used rather than the TPS7A16A-Q1 regulator.