STDA036 October 2026 AFE7769D , AFE7920 , AFE8030 , AFE8092 , AFE8190 , AFE8192
TI's RFICs feature fast standby/wake-up times to optimize radio system low-power modes while maintaining a 2μs wake-up time in many use cases. In FDD systems, this primarily enables micro-DTX and micro-DRX, and in TDD systems, the features enable maximum channel-disable time of the transmitter during uplink and the receiver during downlink.
Transmitter or downlink level standby can be a primary mechanism for reducing PA power consumption. The PA, which may consume more than 50% of radio unit power, is always the biggest target for energy savings. For FDD systems, the 5G standard introduced micro-DTX which allows the transmitter channel to be deactivated at the OFDM symbol level within data frames. Thus, engineers have more opportunities to put the radio into transmitter standby state during unused slots. Micro-DTX works by putting the power amplifier into a sleep state during empty OFDM symbols. The challenge of actual implementation is the stringent wake-up time of one OFDM symbol duration.
Referring to Figure 2, wake-up all channels simultaneously in a multi-channel radio system can cause large current transients resulting in voltage ripple on RFIC supply rails. This can affect RFIC initial sampling performance due to power rail settling. Power supply designers also have to consider small interval of TDD guard time (not shown in Figure 2) where both uplink and downlink are disabled. This scenario creates even more transients as the current draw goes from high draw to low draw and then to high draw state. Moreover, the power supplies can also have more transient surge loss, therefore compromising the overall system efficiency.
To mitigate these issues, TI's RFICs can wake up in a staggered fashion for individual channels or certain group of channels, where the enable signals for each group of channels are staggered in time (Ts), as shown in Figure 3. Depending on the configuration, the RFICs allow programming the GPIO to control the channel enable signals independently, enabling flexible control of double, quad, or octet levels of channels.
Designers can apply the same standby and wake-up power saving strategy to receiver chain. The main focus for the power saving is the low noise amplifiers (LNAs) in the receiver uplink chain.