STDA053 October   2026 DP83TC813R-Q1 , DP83TC813S-Q1 , DP83TC815-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Problem Statement on Current Legacy Parts Communication Topology and Ethernet Advantage
  6. 3The Ethernet Advantage
  7. 4The Critical Hurdle: Power Delivery in the Ethernet Shift
  8. 5The Answer: Power Over Data Line (PoDL)
  9. 6Implementation Challenges and Mitigation
  10. 7Conclusion

Implementation Challenges and Mitigation

Injecting DC power onto a high-speed data line introduces risks of signal integrity. The addition of a differential mode inductor (DMI) network reduces the differential impedance on the line, which leads to return loss degradation. Imbalances between the two conductors generate common-mode currents, causing mode conversion and elevated electromagnetic emissions. Adding series inductance decreases the differential impedance at the lower frequency end and results in voltage droop performance degradation.

DP83TC815 PoDL Network Example Figure 6-1 PoDL Network Example

Mitigation Strategies

  • Magnetics Selection: Use specialized high-isolation magnetics designed for a PoDL DMI network. The differential impedance and coupling factors of a DMI network have a significant role in PoDL performance.

    Increasing the inductor value of a DMI network helps with return loss and voltage droop. A DMI network typically adds extra differential impedance at the lower frequency end. Increasing the inductor value shifts the differential impedance degradation to the lower frequency range and prevents any effect at the operating frequency range.

    A coupling inductor DMI network selection reduces the mode conversion factor when compared to a two isolate inductor DMI network. A coupling DMI network filters out any common mode noise on the line to help with mode conversion. Furthermore, a two isolated inductor DMI network typically has some tolerance difference between the two. Having a higher coupling factor further reduces the differential noise and provides a better mode conversion measurement. Another advantage of coupling a DMI network also has by adding mutual factors which increases the differential inductance or impedance on the line.

    DP83TC815 Impedance Calculation
                            for PoDL Network Figure 6-2 Impedance Calculation for PoDL Network
    However, a higher inductor value typically has lower current support on a DMI network. If customers want better signal performance with high current support applications, increasing the size of the DMI network is the tradeoff for the DMI network:
  • Power Loss Optimization: In the high-voltage system of a radar application, there is always a concern about the extra power consumption across the CMT network. For example, in the 48V system, there is always an extra power consumption V2/R across both the PSE and PD board. However, the following PoDL designs in Figure 6-3 and potentially help with this power loss scenario.
DP83TC815 Figure 6-3
Figure 6-4 Design 1 and Design 2 of a PoDL Network to Resolve Power Loss
DP83TC815
  • Design 1 (left figure): Moves the common-mode termination before the AC coupling capacitors. This design eliminates the power loss at the common-mode termination, removing the loss across that termination entirely.
  • Design 2 (right figure): Connects both wires to the positive power supply and uses the cable shield as the ground reference. This design also eliminates the power loss across the common-mode termination and is the approach typically used with shielded cables.
  • PCB layout optimization: For a rigorous decoupling network optimization and controlled impedance routing, follow the layout instruction to further improve signal integrity performance:
    • Place the DMI (differential mode inductor) network with the same layer as the MDI line.
    • Connect vias directly on the DMI footprint and route the vias with the MDI line on the top layer.
    • Minimize the stubs between the DMI and MDI lines.
    • Prevent the vias from being too close to the DMI to prevent any impedance drop and mode conversion.
    • Connect the power and ground polygon pour place in the bottom layer with the DMI network.
    • Void under the DMI and CMC network.
    • TI recommends placing a common mode termination on the bottom layer.
    • Keep the MDI lines and DMI network symmetrical.

  • DP83TC815 PoDL Layout
                            Recommendation Figure 6-5 PoDL Layout Recommendation

  • Additional Implementation Concerns for a PoDL Network:
    • Cable Selection: Cables must be rated for both the differential impedance (100Ω) required by Ethernet and the current carrying capacity required by the PoDL load.
    • Safety and Reliability: The implementation must adhere to stringent automotive safety standards (ISO 26262) to prevent a power fault from compromising the data integrity of the safety-critical sensing stream. Implement the use of a PSE source device to stop power transfers when there is an overcurrent or undercurrent flow, an unexpected classification, reverse voltage, or current protection.