SWRA662A January 2020 – September 2022 AWR1243 , AWR1443 , AWR1642 , AWR1843 , AWR1843AOP , AWR2243 , AWR6843 , AWR6843AOP , IWR1443 , IWR1642 , IWR1843 , IWR6443 , IWR6843 , IWR6843AOP
This white paper discusses the problem of radar-to-radar interference and how it can be managed in TI radar devices. Interference is a major issue for reliable radar functioning, as the number of deployed radars has increased in both automotive and industrial contexts. Thus, the likelihood that one radar’s transmission is received by another radar has also increased. Interference results in a host of issues, such as a degradation in the noise floor leading to missed detections, or blind spots at certain ranges or directions. It can also create ghost objects in certain cases (ghost targets are targets seen by the radar which do not exist).
This paper is only concerned with cases where FMCW radars interfere with each other.
The information presented here covers the following topics: