SWRS326A December 2024 – December 2025 IWRL6844
PRODUCTION DATA
All digital IO pins of the device (except NRESET) are non-failsafe; hence, care needs to be taken that they are not driven externally without the VIO supply being present to the device.
LVDS interface is intended for debugging and development purposes, not for production use
T13 and C17 pins also serves as a Sense On Power lines and impacts boot mode SOP0 and SOP1 respectively. For more details refer to the Pin Attributes.