SWRU467A February 2017 – June 2018 CC3120
To compile the project, select Rebuild solution, as shown in Figure 35.
Figure 35. SimpleLink™ Studio Solution When the build is finished, there will be three succeeded projects (see Figure 36).
Figure 36. SimpleLink™ Studio Compiled Solution To start debugging, run the debugger (see Figure 37).
Figure 37. SimpleLink™ Studio Debugger A command line window opens and you can see the message printing as the application executes (see Figure 23).