SWRU558 June 2020 CC3100 , CC3100MOD , CC3200 , CC3200MOD
| Argument | com |
| Description | Indicates the COM port to be used when connecting to the device |
| Options | Decimal number indicating the COM port |
| Default | N/A |
| Required? | Yes, can also be set on the *.usf |
| Argument | imagePath |
| Description | Indicates the path to the Image file |
| Options | String of the full path (insensitive to '/' or '\') |
| Default | N/A |
| Required? | Yes, can also be set on the *.usf |
| Argument | debug |
| Description | Verbose mode for printing additional information |
| Options | [true, false] |
| Default | False |
| Required? | Yes, can also be set on the *.usf |
| Argument | Capacity |
| Description | Serial flash capacity for format operation |
| Options | [512KB, 1MB, 2MB, 4MB, 8MB, 16MB] |
| Default | 1MB |
| Required? | Yes, can also be set on the *.usf |
| Argument | spPath |
| Description | Indicates the path to the service pack file |
| Options | String of the full path (insensitive to '/' or '\') |
| Default | N/A |
| Required? | Yes, can also be set on the *.usf |
| Argument | imageVerify |
| Description | Image verification after programming. Linux only |
| Options | [true, false] |
| Default | False |
| Required? | Yes, can also be set on the *.usf |