SWRU558 June 2020 CC3100 , CC3100MOD , CC3200 , CC3200MOD
Image programming of the device is applied upon clicking the 'Image Programmig' button. Another way is from the top bar by clicking Operation → Image Programming. Uniflash then requires the binary image created by Export operation. Please note that the full sized image is required and not the IntelHex format binary.
Figure 46. Programming Button