SWRU558 June 2020 CC3100 , CC3100MOD , CC3200 , CC3200MOD
The Remove button enables the user to remove any command from the image. Also multiple commands can be removed using multiple selections as shown in Figure 42. Also note that it is possible to remove commands by selecting items and pressing the delete button on the keyboard.
Figure 42. Multiple Remove