SWRU558 June 2020 CC3100 , CC3100MOD , CC3200 , CC3200MOD
Figure 27 shows a screenshot of all the mDNS Client parameters. Some parameters have default values in case the user decides to skip configuration. However, mDNS services are mostly user specific and require the user configuration. There are two relevant screens: the main screen and per service screen. In the main screen, the following parameters are defined:
Figure 27. Mdns Main Screen In the service screen, the following parameters are defined for service #1:
Figure 28. Mdns Configuration