SWRU647 September 2026
J5 connector provides access to the onboard XDS110 (TM4C1294NCPDT) emulator. This connection provides the following interfaces to the PC:
When used in standalone mode of operation, the power is supplied through a single USB connector. Connector J5 is also used for configuration and data transfer through the user UART mounted on PC by XDS110 interface. When enumerated correctly, the two UART ports from the XDS110 are displayed on the device manager as a virtual COM Port, similar to that shown in Figure 2-29.
Figure 2-29 Virtual COM PortIf the PC is unable to recognize the above COM ports, install the latest EMUpack.