In this build, the board is excited in open-loop fashion with a specified frequency that can be changed through the watch window. The frequency is controlled with the CLLLC_pwmPeriodRef_pu variable. The power flow is from the secondary side to the primary side. Set the load current above 1 A to avoid the unregulated output voltage in open loop.
- Run the project by clicking the Resume button in the Tool Bar
- Set the load current below 2 A during start up
- Clear the trip by writing “1” to the CLLLC_clearTrip variable in the watch window
- Now, slowly increase the input VSEC DC voltage from 0 V to 48 V. Make sure CLLLC_vSecSensed_Volts displays the correct values in the watch window
- The VPRIM variable shows a voltage of close to 400 V per the tank gain designed. Verify that CLLLC_vPrimSensed_Volts shows the correct voltage.
- Test to see operation under different frequencies (that is, above resonance, below resonance)