TIDUCL3 February 2017
The benefit of this TI Design is how linearly and accurately the current through the LEDs follows the temperature as shown in Figure 25.
Figure 25. Thermal Foldback Tested Note that the calculated data is based on the clamp of the IADJ pin set to 2.25 V. This can vary as per the datasheet; however, the slopes of the line when they are decreasing are different by 0.225 and the linearity of the slop is 0.9998. As discussed in Section 7.6, the slope, starting point, and bottom clamp of this graph can all be manipulated in order to create the desired foldback response.