TIDUEV4B December 2019 – November 2025
Figure 2-16 shows the reset scheme for this project. The TPS3808 voltage supervisor senses the VSNS voltage from the coin-cell. Unless the coin-cell is inserted, the TPS3808 supervisor prevents the PMIC from turning on. This is critical to make sure the power-up sequence is correct.
The TPS3808 device has the input MR# connected to RESET Switch and watch dog from processor. If any of the inputs de-asserts (logic low), then this disables the PMIC. Once the reset and VSNVS is stable along with all the power outputs, the PGOOD pin deasserts the Power-ON Reset (POR_B).
Figure 2-16 Reset Scheme With TPS3808 Supervisor